MCUXpresso Config Tools for Local PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Config Tools for Local PC

ソリューションへジャンプ
4,922件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi,

 

I have same problem for MCUXpresso Config Tools for my local PC. I have no internet. After I get error shown in below link. I installed local version of MCUXpresso Config Tools. But error is still exist. Could you help me please?

 

link:https://community.nxp.com/t5/MCUXpresso-General/Cannot-open-MCUXpresso-Config-tools-from-V11-1/td-p/...

Thanks and Regards.

0 件の賞賛
返信
1 解決策
4,876件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

The latest detailed steps for downloading the data can be found in this thread :

https://community.nxp.com/t5/MCUXpresso-Config-Tools/Why-config-tools-always-show-no-internet-link-a...

Regards

Petr Hradsky

Config Tools Team

元の投稿で解決策を見る

6 返答(返信)
4,900件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi Dear @marek-trmac 

 

I could not see the section you mention. I also tried below link directives but result is fail. Error still exist. Could you help me please ?

Thanks and Regards.


Link:https://community.nxp.com/t5/MCUXpresso-Config-Tools/How-to-Use-MCUXpresso-Config-Tools-on-Offline-C...

Doc:https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/mcuxpresso-config%40tkb/30/1/How%20to%20...

0 件の賞賛
返信
4,917件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Lukas,

go to https://mcuxpresso.nxp.com and download offline data for selected processor, see link "MCUXpresso Config Tools - Offline data" on the left side.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
4,877件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

The latest detailed steps for downloading the data can be found in this thread :

https://community.nxp.com/t5/MCUXpresso-Config-Tools/Why-config-tools-always-show-no-internet-link-a...

Regards

Petr Hradsky

Config Tools Team

4,867件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi Dear @Petr_H ,

 

I just want to clear my mind for one issue. In my local pc, I installed MCUXpresso but MCUXpresso Config not installed automatically. Was it required to installed as built in with defaultly? Or, do I need to installed it manually? I asked this because when I installed externally I get the same error.

Thanks and Regards.

 

 

0 件の賞賛
返信
4,853件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello Lukas,

>> I installed MCUXpresso but MCUXpresso Config not installed automatically

Did you install MCUXpresso IDE or MCUXpresso Config Tools (stand alone)?

 

If you installed MCUXpresso IDE, can you attach here <workspace>/.metadata/.log

If you installed MCUXpresso Config Tools, can you attach here the <HOME>/.nxp/swtools.log

So we can look what is wrong? There's high chance the root cause is logged there.

 

Regards,

Libor

4,829件の閲覧回数
Lukas_Frank
Senior Contributor I

Dear @liborukropec 

 

Previous reply handle the issue. Thanks for support and interests..

0 件の賞賛
返信