LPC5536, is 64 pin version supported?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5536, is 64 pin version supported?

Jump to solution
3,386 Views
AlbertoGarlassi
Contributor II

Hello, first time user of MCUXpresso so please bear with me.

I can't find how to use the very useful pin configuration tool for anything other than the 100 or 48 pin variant.

It seems the 64 pin package is not available in the SDK. 

Sorry for the lame question.

 

Alberto

0 Kudos
Reply
1 Solution
3,370 Views
tomasklir
NXP Employee
NXP Employee

Hi @AlbertoGarlassi ,

for a new configuration you can choose the desired package:

tomasklir_0-1689841138114.pngtomasklir_0-1689841138114.png

For an existing configuration, select File->Switch Package.

Best Regards,

Tomas Klir

View solution in original post

3 Replies
3,356 Views
AlbertoGarlassi
Contributor II

Thanks for the prompt reply, for some reason I was looking for it in the IDE.

Regards

Alberto

0 Kudos
Reply
3,314 Views
tomasklir
NXP Employee
NXP Employee

In IDE you can also select it in the new project wizard

tomasklir_0-1689949418850.pngtomasklir_0-1689949418850.png

or afterwards in the Project Explorer

tomasklir_1-1689949473352.pngtomasklir_1-1689949473352.png

 

Best regards,

Tomas Klir

 

0 Kudos
Reply
3,371 Views
tomasklir
NXP Employee
NXP Employee

Hi @AlbertoGarlassi ,

for a new configuration you can choose the desired package:

tomasklir_0-1689841138114.pngtomasklir_0-1689841138114.png

For an existing configuration, select File->Switch Package.

Best Regards,

Tomas Klir