Importing current project in IDE to Config tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Importing current project in IDE to Config tool

ソリューションへジャンプ
2,436件の閲覧回数
benjamin_miller
Contributor I

I am currently using a FRDM-KL27z board and am having trouble setting up my current project in my MCUXpresso IDE to the MCUXpresso config tool. Anyone know how to connect an existing project in the IDE to the config tool? I have tried setting up a new config in the desktop application and have also tried clicking the 'open pins' button on the IDE, but get the error message "Processor 'MKL27Z64xxx4 is not supported or data for processor not available (check internet connection)"

1 解決策
2,228件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello Benjamin,

are you behind proxy or without internet connectivity? The Config Tools need to download some data when the tools configuration is created. Once downloaded, it is used from the cache directory, unless you create a configuration for different processor.

Regards,

Libor

元の投稿で解決策を見る

2 返答(返信)
2,229件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello Benjamin,

are you behind proxy or without internet connectivity? The Config Tools need to download some data when the tools configuration is created. Once downloaded, it is used from the cache directory, unless you create a configuration for different processor.

Regards,

Libor

2,228件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I just tested it with MCUXpresso IDE 10.2.0 and FRDM-KL27Z SDK2.4.0. I didn't find any problem. see attached video.

Did you download the latest SDK2.4.0?

pastedImage_1.png
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信