How to get ENET into ConfigTools Peripherals list?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get ENET into ConfigTools Peripherals list?

ソリューションへジャンプ
2,212件の閲覧回数
jeffthompson
Contributor V

I'm using MCUXpresso IDE 11.0.1 for an MIMXRT1062DJ6A. I started with the SDK example code for host_cdc_bm (which I ported to FreeRTOS). I now need to add the ENET peripheral and started by adding the ENET driver. When I go to the ConfigTools Peripherals, ENET does not appear in the list.

タグ(1)
1 解決策
2,105件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Jeff Thompson,

Unfortunately, the ENET module is not supported by the ConfigTools Peripherals. However, you can use the ENET examples from the SDK as a starting point for your project.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,106件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Jeff Thompson,

Unfortunately, the ENET module is not supported by the ConfigTools Peripherals. However, you can use the ENET examples from the SDK as a starting point for your project.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------