Error in Config Tools for FlexCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in Config Tools for FlexCAN

ソリューションへジャンプ
2,231件の閲覧回数
stefano-quantic
Contributor III

In: Config Tools | Peripherals | Peripheral drivers (device specific) | FLEXCAN | Flexcan general configuration | FlexCAN configuration

there is a setting named "Self Reception" (the 14th settings of this block; it's a checkbox).
It should be renamed "Disable Self Reception", since its value determines the value of flexcan_config_t.disableSelfReception in the generate code (in peripherals.c), which in turn determines the setting for FlexCAN's bit MCR[SRXDIS].
The current name suggests the exact opposite of what it does, so it's very confusing.

This is for a project using iMXRT1176.

0 件の賞賛
返信
1 解決策
2,163件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

Thank you for reporting the issue. You are right that the name of the setting is confusing and should be fixed.

I have already created a ticket to fix the issue in the next release of MCUXpresso Config Tools.

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,164件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

Thank you for reporting the issue. You are right that the name of the setting is confusing and should be fixed.

I have already created a ticket to fix the issue in the next release of MCUXpresso Config Tools.

Best Regards,

Marek Neuzil

0 件の賞賛
返信