On MCUXpresso IDE I created a new project using the wizard and selecting "Makefile Project with Existing Code".
Then when I attempt to use MCUXpresso Config tool, I get the error message: There is no core selected
and it won't generate any code.
I'm using MCUXpresso v11.0.0 on MAC OSX
CPU is LPC55S69 - which is dual core!
I guess the wizard failed to set some attribute that config tool uses.
Is there some way I can set this manually?
I've had a look through the MCU 'Edit' menu and all I can see is menu to set 'package' and 'chip'.
Comparing my Makefile project settings with the 'hello world' example, MCU settings for 'core' and 'processor' are set in 'hello world' but not in the project I created from Makefile.
See attached screenshots.