Create new Config tool chain can not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create new Config tool chain can not found

2,018 Views
EricWlin
Contributor I

1. Create a new configuration and project based on the SDK instance or Hello Word project  

2. D:\SDK_2_10_1_MIMXRT1170-EVK     ok

3. tool chain : It is not possible to select (show  MCUXpresso IDE)

What should I do? thank youSnipaste_2021-11-22_16-56-06.png

0 Kudos
Reply
1 Reply

2,012 Views
marek-trmac
NXP Employee
NXP Employee

Hi EricWin,

Config Tools are integrated into MCUXpresso IDE. Stand-alone version of Config Tools are expected to be used with third party toolchains, like IAR, Keil MDK or ARM GCC.

Open SDK example in MCUXpresso IDE. Right on the project in Project Explorer and select "MCUXpresso Config Tools > Open Tools Overview"

Regards, Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button