ConfigTools I2C setup error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ConfigTools I2C setup error

3,076 Views
popkov
Contributor I

Setting pins to I2C mode enables push-pull mode by default, while open-drain mode is required for normal I2C operation.

Pins version: v7.0

Tags (2)
0 Kudos
Reply
4 Replies

2,944 Views
Petr_H
NXP Employee
NXP Employee

Hi,

Currently the "electrical features" settings, such as open-drain, are not handled automatically in the Pins tool. Their adjustment now has to be done by user. Thank you for the feedback, we will consider this improvement for the next versions of the tool.

best regards

Petr Hradsky

MCUXpresso config tools team

0 Kudos
Reply

2,944 Views
popkov
Contributor I

Got it.

Thanks, Petr.

0 Kudos
Reply

2,944 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

Hope you are doing well. Could you please confim the microcontroller that you are using, so that I may check if it happens with others too.

Best Regards,

Sabina

0 Kudos
Reply

2,944 Views
popkov
Contributor I

Hello.

MCU is Kinetis MKV58F1M0xxx24.

0 Kudos
Reply