ConfigTools I2C setup error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ConfigTools I2C setup error

3,097件の閲覧回数
popkov
Contributor I

Setting pins to I2C mode enables push-pull mode by default, while open-drain mode is required for normal I2C operation.

Pins version: v7.0

タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,965件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

Currently the "electrical features" settings, such as open-drain, are not handled automatically in the Pins tool. Their adjustment now has to be done by user. Thank you for the feedback, we will consider this improvement for the next versions of the tool.

best regards

Petr Hradsky

MCUXpresso config tools team

0 件の賞賛
返信

2,965件の閲覧回数
popkov
Contributor I

Got it.

Thanks, Petr.

0 件の賞賛
返信

2,965件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

Hope you are doing well. Could you please confim the microcontroller that you are using, so that I may check if it happens with others too.

Best Regards,

Sabina

0 件の賞賛
返信

2,965件の閲覧回数
popkov
Contributor I

Hello.

MCU is Kinetis MKV58F1M0xxx24.

0 件の賞賛
返信