Clocks diagram - which project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clocks diagram - which project?

ソリューションへジャンプ
6,393件の閲覧回数
JBM
Contributor V

I have a workspace with multiple projects and the clocks diagram shows the same thing no matter which project is selected.  One is a static library without clocking.  I know the projects aren't all the same.  

Am I missing something?  Shouldn't the clocks diagram show the configuration for the selected project?

I am running MCUXpresso v11.4.0 [Build 6224].  The chip is the K64FN1M0VDC12.

0 件の賞賛
返信
1 解決策
6,359件の閲覧回数
JBM
Contributor V

Thanks that works.  If I open the clocks and then go back to the code editor and expand the clocks diagram it is updated.

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
6,365件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi James,

Erich is right, if you have more projects, you have to open to proper one. The MCUX Config Tools allows to have just one configuration to be opened, so if you have more Eclipse projects, you have to explicitly switch/select the project you want to work with. Either in the Config Tools perspective as Erich proposed, or in the Develop perspective, in the Project Explorer view:

liborukropec_0-1655903861655.png

 

or even popup menu on the project folder.


Regards,

Libor

6,358件の閲覧回数
ErichStyger
Specialist I

My preferred way is to double-click on the .mex in the project to open that as the configuration I want to use/change:

ErichStyger_0-1655904171346.png

 

0 件の賞賛
返信
6,360件の閲覧回数
JBM
Contributor V

Thanks that works.  If I open the clocks and then go back to the code editor and expand the clocks diagram it is updated.

0 件の賞賛
返信
6,378件の閲覧回数
ErichStyger
Specialist I

did you switch/select your project already here:

ErichStyger_0-1655869514222.png

 

?

タグ(1)
0 件の賞賛
返信
6,357件の閲覧回数
JBM
Contributor V

tempsnip.png

 

Strange - I don't have that combo box to select from.  If I right click on the toolbar and select "Restore Hidden Toolbar Entries", it doesn't show up.  I don't see where that option is.

0 件の賞賛
返信
6,344件の閲覧回数
liborukropec
NXP Employee
NXP Employee

The combo is part of toolbar in MCUX Config Tools perspective(s). If you open a view in another perspective, this won't be shown. I believe it is your case.

Libor

0 件の賞賛
返信
6,341件の閲覧回数
JBM
Contributor V

Thanks - that is what's happening.  I have the Clocks Diagram open in the Develop Perspective and that is not shown.  If I open it in the Clocks perspective, I can select the project.

Thanks again everybody!

0 件の賞賛
返信
6,353件の閲覧回数
ErichStyger
Specialist I

Check this:

ErichStyger_0-1655906196182.png

 

0 件の賞賛
返信
6,322件の閲覧回数
JBM
Contributor V

It was checked.  The problem is that you can open the clocks diagram within the development perspective and then that toolbar option isn't shown.  You're left with a clocks diagram and no way to select what the project is.

0 件の賞賛
返信