v2 KBOOT support for MKV58F24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

v2 KBOOT support for MKV58F24

1,985件の閲覧回数
adamwozniak
Contributor I

v2 KBOOT seems to have support for the MKV58F22 but not the MKV58F24.  Has anyone done this work?  Is there a big difference between these chips?  Will the F22 bootloader "just work" on the F24? I don't want to have to reinvent the wheel.

ラベル(1)
0 件の賞賛
返信
1 返信

1,742件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Adam Wozniak,

In my opinion, the MKV58F22 can be regarded as the enhanced MKV58K22 and they're compatible with each other.

So the demo MKV58F22 is suit for the MKV58F24, however I'd high recommend you to do some porting work by referring to the Chapter 10 in the attachment.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信