uTaskerSerialBootloader on S9KEAZN64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uTaskerSerialBootloader on S9KEAZN64

1,165件の閲覧回数
curiosul
Contributor III

Hello!

I was trying in to build and upload an Kinetis Bootloader 1.2 on the respective MCU but with no success! I find impossible to adapt official bootloader to this MCU family. As an alternative I proceed with uTaskerSerialBootloader. As I have read, when KBOOT_LOADER is enabled, it should be compatible with Kinetis Updater application!

I have followed the indications from the guide: http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF 

I have tested the following two configuration in config.h one by one:

#define FRDM_KEAZ64Q64
#define TRK_KEA64‍‍‍‍

As the board I am working with is a custom one, I have also forced bootloader mode this way:

#define FORCE_BOOT()       (1)‍

I have followed the manual when I imported the project and everything seems to be fine!

I have also checked baudrates and other UART configuration in app_hw_kinetis.h and the port is selected correctly connected!

Does anyone have experience with this? Is there any other special requirement to do make it works?

Thanks!

タグ(2)
0 件の賞賛
返信
0 返答(返信)