Why the r1 register always equal _extext address when copy none cachable region and ramfunction region to RAM in RT062 startup file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why the r1 register always equal _extext address when copy none cachable region and ramfunction region to RAM in RT062 startup file

1,708 Views
zhoujiazhao
Contributor I

nxpftftechforum

Question about  r1 register

Enable __PERFORMANCE_IMPLEMENTATION, __STARTUP_INITIALIZE_RAMFUNCTION and __STARTUP_INITIALIZE_NONCACHEDATA  macro.

Why the r1 register always equal _extext address when copy none cachable region and  ramfunction region to RAM.

Copy none cachable region to RAM:

In subs r3,#4 instruction,  get the offset address base on __NDATA_ROM(defined in .ld file) to r3;

In ldr r0, [r1, r3]  instruction,  r0 = r1 + r3, at this moment, r1=__etext(the r1 not change after ldr r1,=__text instruction);

?????????  Why r1 is __etext address rather than __NDATA_ROM address????????????????

Copy ramfunction region to RAM:

?????????  Why r1 is __etext address rather than start ROM address of ramfunction region????????????????

/* Reset Handler */

    .thumb_func
    .align 2
    .globl   Reset_Handler
    .weak    Reset_Handler
    .type    Reset_Handler, %function
Reset_Handler:
    cpsid   i               /* Mask interrupts */
    .equ    VTOR0xE000ED08
    ldr     r0, =VTOR
    ldr     r1, =__isr_vector
    str     r1, [r0]
    ldr     r2, [r1]
    msr     mspr2
#ifndef __NO_SYSTEM_INIT
    ldr   r0,=SystemInit
    blx   r0
#endif
/*     Loop to copy data from read only memory to RAM. The ranges
 *      of copy from/to are specified by following symbols evaluated in
 *      linker script.
 *      __etext: End of code section, i.e., begin of data sections to copy from.
 *      __data_start__/__data_end__: RAM address range that data should be
 *      __noncachedata_start__/__noncachedata_end__ : none cachable region
 *      __ram_function_start__/__ram_function_end__ : ramfunction region
 *      copied to. Both must be aligned to 4 bytes boundary.  */

    ldr    r1, =__etext
    ldr    r2, =__data_start__
    ldr    r3, =__data_end__

#ifdef __PERFORMANCE_IMPLEMENTATION
/* Here are two copies of loop implementations. First one favors performance
 * and the second one favors code size. Default uses the second one.
 * Define macro "__PERFORMANCE_IMPLEMENTATION" in project to use the first one */
    subs    r3r2
    ble    .LC1
.LC0:
    subs    r3#4
    ldr    r0[r1, r3]
    str    r0[r2, r3]
    bgt    .LC0
.LC1:
#else  /* code size implemenation */
.LC0:
    cmp     r2r3
    ittt    lt
    ldrlt   r0, [r1], #4
    strlt   r0, [r2], #4
    blt    .LC0
#endif
#ifdef __STARTUP_INITIALIZE_RAMFUNCTION
    ldr    r2, =__ram_function_start__
    ldr    r3, =__ram_function_end__
#ifdef __PERFORMANCE_IMPLEMENTATION
/* Here are two copies of loop implementations. First one favors performance
 * and the second one favors code size. Default uses the second one.
 * Define macro "__PERFORMANCE_IMPLEMENTATION" in project to use the first one */
    subs    r3r2
    ble    .LC_ramfunc_copy_end
.LC_ramfunc_copy_start:
    subs    r3#4
    ldr    r0[r1, r3]
    str    r0[r2, r3]
    bgt    .LC_ramfunc_copy_start
.LC_ramfunc_copy_end:
#else  /* code size implemenation */
.LC_ramfunc_copy_start:
    cmp     r2r3
    ittt    lt
    ldrlt   r0, [r1], #4
    strlt   r0, [r2], #4
    blt    .LC_ramfunc_copy_start
#endif
#endif /* __STARTUP_INITIALIZE_RAMFUNCTION */
#ifdef __STARTUP_INITIALIZE_NONCACHEDATA
    ldr    r2, =__noncachedata_start__
    ldr    r3, =__noncachedata_init_end__
#ifdef __PERFORMANCE_IMPLEMENTATION
/* Here are two copies of loop implementations. First one favors performance
 * and the second one favors code size. Default uses the second one.
 * Define macro "__PERFORMANCE_IMPLEMENTATION" in project to use the first one */
    subs    r3r2
    ble    .LC3
.LC2:
    subs    r3#4
    ldr    r0[r1, r3]
    str    r0[r2, r3]
    bgt    .LC2
.LC3:
#else  /* code size implemenation */
.LC2:
    cmp     r2r3
    ittt    lt
    ldrlt   r0, [r1], #4
    strlt   r0, [r2], #4
    blt    .LC2
#endif
/* zero inited ncache section initialization */
    ldr r3, =__noncachedata_end__
    movs    r0,0
.LC4:
    cmp    r2,r3
    itt    lt
    strlt   r0,[r2],#4
    blt    .LC4
#endif /* __STARTUP_INITIALIZE_NONCACHEDATA */

#ifdef __STARTUP_CLEAR_BSS
/*     This part of work usually is done in C library startup code. Otherwise,
 *     define this macro to enable it in this startup.
 *
 *     Loop to zero out BSS section, which uses following symbols
 *     in linker script:
 *      __bss_start__: start of BSS section. Must align to 4
 *      __bss_end__: end of BSS section. Must align to 4
 */
    ldr r1, =__bss_start__
    ldr r2, =__bss_end__

    movs    r00
.LC5:
    cmp     r1r2
    itt    lt
    strlt   r0, [r1], #4
    blt    .LC5
#endif /* __STARTUP_CLEAR_BSS */

    cpsie   i               /* Unmask interrupts */
#ifndef __START
#define __START _start
#endif
#ifndef __ATOLLIC__
    ldr   r0,=__START
    blx   r0
#else
    ldr   r0,=__libc_init_array
    blx   r0
    ldr   r0,=main
    bx    r0
#endif
    .pool
    .size Reset_Handler, . - Reset_Handler
0 Kudos
Reply
1 Reply

1,669 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi jiazhao,

yes, this code seems have problem. Please change r1 according to the ld file.

Thanks,

Jing

0 Kudos
Reply