Makefile fix when cross-compiling blhost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Makefile fix when cross-compiling blhost

2,533件の閲覧回数
damiendusha
Contributor II

Just a quick note to others that may be in the same position.

When attempting to cross-compile blhost on Linux with the KBOOT 2.0.0 package, linking will likely fail using the supplied host file.  Even where it does succeed, there might be host contamination.

 

The attached patch will fix this problem, so long as the environment variable CXX is correctly set.

Original Attachment has been moved to: 0001-Make-LD-use-CXX-rather-than-native-g.patch.zip

タグ(3)
0 件の賞賛
返信
1 返信

1,998件の閲覧回数
higor
Contributor II

Can you help me with this cross compilation?

0 件の賞賛
返信