MCUBoot for K32L2B?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUBoot for K32L2B?

1,413 次查看
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

I'm looking for the MCUBoot middleware for K32L2Bxxx but couldn't find it in SDK 2.6.0

Are there plans to integrate in in future releases of the SDK?

Second question: Can MCUBoot be used for image verification (via a signature) to allow only valid images to be flashed via MCUBoot?

br

Guenter 

0 项奖励
回复
1 回复

1,296 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Guenter Loettrich ,

   K32L2Bxxx already contains the ROM bootloader:

pastedImage_1.png

   That's why the SDK didn't contains the MCUBOOT middleware.

   If you want to use the related tools, eg. blhost, elftosb,etc.

   You can go to the NXP mcuboot page download it:

MCU Bootloader | NXP 

  You can try to use the KinetisFlashTool tool to download the code.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you h

0 项奖励
回复