LPCXpresso54628 No Meil Build *.BIN To Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso54628 No Meil Build *.BIN To Bootloader

1,618件の閲覧回数
spu12kimo
Contributor I

How do I need to burn to LPCXpresso54628 without using Meil build to * .bin through YModem file transfer protocol?
Is it OK to use only MCUXpresso IDE?
Thank 

0 件の賞賛
返信
1 返信

1,518件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hello 寶凱 李, 

I suppose that you are using the AN12384  LPC5460x UART Secondary Bootloader using YModem, which illustrates

how to build your bin file using Keil IDE. To use MCUxpresso you will need to port your source files into a new project and use its tools to generate the bin file.


Have a great day,
Diego

-------------------------------------------------------------------------------

Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信