LPC1518JBD64 Programming Spec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1518JBD64 Programming Spec

ソリューションへジャンプ
3,470件の閲覧回数
Leap_Electronic
Contributor II

This is Alex from Leaptronix.

We are the third party of programmer.

Could we apply below IC programming spec

LPC1518JBD64

Thanks and have a good day.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,355件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ryan Tseng,

  You are welcome.

  So, please help to mark the correct answer or assumed answered item, just to close this question, thank you!

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,355件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ryan Tseng ,

  This community block is mainly used for the kinetis, if you have the LPC question, you can post your question in this area:

 LPC Microcontrollers 

  LPC1518JBD64 is the Cortex M3 core, so you can check the ARM core SWD/JTAG programmer, and the LPC1518JBD64 flash operation in the user manual.

If you have more questions, please create your question in the LPC area, the LPC engineer will help you in details.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,355件の閲覧回数
Leap_Electronic
Contributor II

Thanks for the respond and help.

I will post in the LPC area.

0 件の賞賛
返信
3,356件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ryan Tseng,

  You are welcome.

  So, please help to mark the correct answer or assumed answered item, just to close this question, thank you!

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信