LPC13xx SWD Programe MCU Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC13xx SWD Programe MCU Flash

2,464 次查看
Luoyin
Contributor I

Hello,

Our company is design the programer, Local in Guangzhou China(www.up48.com).

Now, We are try to add the NXP LPC13xx to our device. Via the swd to programe the mcu flash.

But we can't find the doc about the FMC Register description.  

 

0 项奖励
回复
4 回复数

2,413 次查看
Luoyin
Contributor I

Thank very much.

0 项奖励
回复

2,450 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to section 21.16 Flash controller registers, especially FLASHCFG register for flash delay configuration.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1710123724076.png

 

0 项奖励
回复

2,435 次查看
Luoyin
Contributor I

Hello, thank !

Yes, I note that before, But it no detail description.

For example, how to set the REG to erase the chip, program the flash and unlock chip, etc.

I thank, It should be have a doc to describe.

 

0 项奖励
回复

2,430 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For Flash programming operation, pls refer to section in UM10524.pdf:

21.14 IAP commands

There is code in ROM, which provides flash eraing/programming api function, you can call them.

Hope it can help you

BR

XiangJun Rong

 

 

0 项奖励
回复