KL27 connection via USB to KinetisFlashTool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL27 connection via USB to KinetisFlashTool

ソリューションへジャンプ
3,419件の閲覧回数
brock
Contributor II

We have a KL27 soldered onto a custom USB board.

 

The new KinetisFlashTool won't connect directly to this chip via USB-HID, even though it shows up properly in the Device Manager as an HID device with the correct VID and PID values.

 

Is the bootloader that ships inside each device supposed to connect to the KinetisFlashTool?

 

Is there some trick to get it to connect the first time?

ラベル(1)
1 解決策
3,176件の閲覧回数
brock
Contributor II

We got this working by trying different WIN 7 machines until it started working with one.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,176件の閲覧回数
bobpaddock
Senior Contributor III

The DOS command line tool BLHOST has worked on every PC.

The Windows GUI tools works only on random PCs I've tried. :-(

There is something that the tool is assuming is present, perhaps a compiler DLL, that when is missing the tool does nothing.

No error, acts like it was never even started.

3,177件の閲覧回数
brock
Contributor II

We got this working by trying different WIN 7 machines until it started working with one.

0 件の賞賛
返信