KE1xF bootloader when execute CRC-32 check on application data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KE1xF bootloader when execute CRC-32 check on application data

1,566件の閲覧回数
isaotakashima
Contributor IV

The KE1xF ROM bootloader support CRC-32 check on application data feature.

I think that the ROM bootloader execute CRC-32 check on application data before jump to user application.

If CRC-32 check failed, the ROM bootloader assert PTA11.

Therefore this feature only available when BOOTSRC_SEL (FOPT[7])  = 1.

Is my understanding correct?

Please reply as soon as possible.

Best regards,

Takashima

0 件の賞賛
返信
2 返答(返信)

1,332件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check Kinetis product team feedback below:

The customer understanding is right. Only when boot from ROM, the ROM bootloader can implement the CRC32, to check the image located in the flash. Whether implement the CRC32 depends on the BCA configurations. By default, the BCA (start from Flash address 0x3C0) are all 0xFF, so ROM bootloader will read its own default BCA configuration, in which the CRC32 check is disabled.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,332件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Takashima,

I am checking with Kinetis product team and let you know later.

Thank you for the patience.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信