K22 one-pass Bootloader+User Program Install

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22 one-pass Bootloader+User Program Install

2,042件の閲覧回数
gcarlson
Contributor II

For production we would like the be able to pre-program the K22 chips with both the bootloader and the current version of the runtime code in order to reduce the programming and test time on the production line.  Currently we have a programming file for them to use to pre-program the bootloader portion of this, but we aren’t sure how to make a combined binary (or HEX) image that they can then pre-program into the chips.

We are going to use the Bootloader version that remains resident in the K22 (not one-time programming) so we can perform later field updates of the user program

I've been looking at the Kinetis Flash Tool, which permits configuration of the Bootloader Configuration Area, as well as programming the user program into the K22.  But I don't superficially see if a combined programming sequence (Bootloader + User Program) can be programmed in one-pass.

Advice appreciated,

Gordy Carlson

0 件の賞賛
返信
2 返答(返信)

1,749件の閲覧回数
gcarlson
Contributor II

Or to better clarify..... Can the Bootloader and user program be combined into one file that can be programmed into the K22 during the initial manufacturing, regardless of programming tool used?

0 件の賞賛
返信

1,749件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

First of all, sorry for the later reply.

Please refer below document about combine the bootloader and application in one image file.

<<Merging applications using Kinetis Design Studio>>

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信