FRDM-KW38

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW38

5,054件の閲覧回数
CBI
Contributor II

Hi all
I have bought 5 identical products : FRDM-KW38

I have followed user guide as defined in NXP Video: https://www.nxp.com/document/guide/getting-started-with-the-frdm-kw38:GS-FRDM-KW38
I have imported the NXP SDK example shown in this video   frdmkw38_heart_rate_sensor_freertos

After clean, build and launch debug, the FRDM-KW38 is in a bugged state : The firmware has been loaded into the board but I cannot reload again the same firmware. When I want to launch debug, I have a pop-up indicating:

Unable to connect wire for probe index 1.
Error: Wire Ack Fault - target connected?

CBI_0-1614597501700.png


I have taken another board and after the same usage , I have again the same error. How to restart my FRDM-KW38 and loaded correctly another example or remove this error ?

Thanks in advance for your help.
CBI

 

0 件の賞賛
返信
3 返答(返信)

5,029件の閲覧回数
CBI
Contributor II

Hi all

The NXP link is incorrect to Download – OpenSDA Bootloader and Application
In this page : https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial...
the link is for a FRDM-KW36  (not for FRDM-KW38)

On this page, use only Segger Jlink FRDM-KW38 to perform a debug session

CBI_0-1614683750297.png

 

 

5,047件の閲覧回数
CBI
Contributor II

Please help me... always the same problem with my board FDRM-KW38 to start

0 件の賞賛
返信

5,042件の閲覧回数
CBI
Contributor II

I have rebooted my computer (under Windows 10)
I have cleanup the debug
I have deleted the frdmkw38_heart_rate_sensor_freertos project and reload it again
Clean is Ok
Build in debug mode is OK
BUT Impossible to debug again....

I have selected the DAPLink CMSIS-DAP 
CBI_0-1614610854056.png

Then whatever the action =>  here I have choice : check files areas blank

CBI_1-1614610972501.png

The result is : 

CBI_2-1614611154123.png

 

 

 

0 件の賞賛
返信