Does K22F micro controller supports hardware reliable update feature?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does K22F micro controller supports hardware reliable update feature?

2,771件の閲覧回数
swapnilpendhare
Contributor III

Hi, 

 

I went through KBOOT source and found that it's hardware reliable update functionality which uses micro controller's flash SWAP feature. I found no support for flash swap feature (command 0x46) in K22F; which means i can not perform hardware firmware update on K22F microcontroller. 

 

Is my understanding correct or I am missing something here ?

 

Thanks, 
Swapnil Pendhare

ラベル(1)
タグ(3)
1 返信

2,351件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Swapnil Pendhare,

The ReliableUpdate command has supported software and hardware implementations, the hardware approach doesn't work if the device doesn't support the flash swap feature and only option is the software implementations.

2016-10-12_9-48-25.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------