Bootloader for LPC54S018J4MET180E

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bootloader for LPC54S018J4MET180E

2,826 次查看
jackhsu
Contributor III

Hi,

 

I need your help to set up the flash loader via IAR, and plan to create a flash loader to do internal flash programming via SPIFI.

 

I have downloaded the flashloader project and try to run it on IAR.

When I run download and debug via J-Link, and it always stuck in peripheral checking.

WeChat 圖片_20220307164021.png

I guess my hardware design is not compatible the bootloader, and maybe I need to remove some instructions. There is the hardware design on our programming board. Could you help to give us some suggestions?

WeChat 圖片_20220307165056.png

 

0 项奖励
回复
2 回复数

2,764 次查看
jackhsu
Contributor III

Hi Alice,

 

The issue is solved because we modify initialize.

Thanks.

 

0 项奖励
回复

2,787 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

Please first check the external flash work well, you can use spifi demo under SDK.

 

BR

Alice

0 项奖励
回复