Bootloader for K30 using Modbus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bootloader for K30 using Modbus

5,112 次查看
blurblur
Contributor II

Hello,

I am very new to the bootloader protocol. I am not really familiar. I found out that kboot v2 doesnt have k30 example. 

Is there any example that I can use as guideline or at least similiar source code. Please help.

Thanks,

illa

6 回复数

4,858 次查看
blurblur
Contributor II

Hi Jing,

I try to follow using the example that you mention. 

On the step 2 you mention to get the system_MK60D10.c and system_MK60D10.h from SDK folder.  For my case, I do not have any SDK for K30 and I create my own board. How do I generate or create this 2 files. Thanks.

Regards,

illa

0 项奖励
回复

4,858 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

please download k30 KSDK package from https://mcuxpresso.nxp.com/en/select . These files are contained in the package.

Regards,

jing

0 项奖励
回复

4,858 次查看
blurblur
Contributor II

Hi,

Is it okay if I am using the K30DX128xxx10 package for the K30DX128VLL7??

It seems that doesnt have for the VLL7

Thanks,

illa

0 项奖励
回复

4,858 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, it's okay.

Regards,

Jing

4,858 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi norzilah,

yes, there isn't K30 bootloader demo in kboot2.0 package. You have to port other demo to K30. But this is not very difficult. There are guide in Kinetis Bootloader v2.0.0 Reference Manual. There is also many discuss and notes in community. For example, https://community.nxp.com/docs/DOC-341144 

You can use MCUXpresso config tools to create clock tree and pin config file.

Regards,

Jing

4,858 次查看
blurblur
Contributor II

Hi Jing,

Thanks for the answer. I will try using k60 tower example as kick-start.  

Regards,

illa

0 项奖励
回复