kernel panic when booting the s32v234sbc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

kernel panic when booting the s32v234sbc

跳至解决方案
11,014 次查看
nskang
Contributor II

Sorry, i'm not good at using English.

I have a s32v234sbc package and i am trying to boot it with yocto image.

(* VisionSDK_S32V2_RTM_1_5_0_img_yocto.tar.gz)

Used image is yocto origianl image(Image, fsl-s32v234sbc.dtb, u-boot.s32)

however, always kernel panic occurs as below.

please, let me know how to figure out it.

* i already check that kernel panic occurs when loading the seq.ko module.

---------------------------------------------------------------------------------------

U-Boot 2018.07+g21d6118 (Sep 24 2019 - 18:09:50 +0000)

CPU: NXP S32V234 V2.0 at 1000 MHz
Reset cause: Software Functional reset
Board: mpxs32v234-R2
I2C: ready
DRAM: 2 GiB
RTC: PCF85263
All (4) cores are up.
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)

Forcing PCIe to Gen1 operation
phy link never came up
DEBUG_R0: 0x007dc100, DEBUG_R1: 0x08200000
In: serial
Out: serial
Err: serial
** Unable to read file cse.bin **
CSE firmware loading failed
Failed to initialize CSE3 security engine
Net: FEC
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
8767496 bytes read in 416 ms (20.1 MiB/s)
Booting from mmc ...
21981 bytes read in 18 ms (1.2 MiB/s)
## Flattened Device Tree blob at 82000000
Booting using the fdt blob at 0x82000000
reserving fdt memory region: addr=80000000 size=10000
Loading Device Tree to 000000009fff7000, end 000000009ffff5dc ... OK

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 4.19.31-rt18+g9efc51a (oe-user@oe-host) (gcc version 6.3.1 20170509 (Linaro GCC 6.3-2017.06~dev)) #1 SMP Tue Sep 24 18:10:27 UTC 2019
[ 0.000000] Machine model: Freescale S32V234
[ 0.000000] cma: Reserved 32 MiB at 0x00000000fe000000
[ 0.000000] random: get_random_bytes called from start_kernel+0xa4/0x400 with crng_init=0
[ 0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s49688 r8192 d32232 u90112
[ 0.000000] Detected VIPT I-cache on CPU0

.

.

.

.

INIT: version 2.88 booting
[ 1.241503] random: fast init done
[ 1.430363] apex: loading out-of-tree module taints kernel.
[ 1.437668] APEX kernel module - IRQ 34, ID 0, 1 devices loaded.
[ 1.443459] APEX kernel module - IRQ 35, ID 1, 2 devices loaded.
[ 1.687735] Managing the chunk [0x89000000 - 0x8fd00000]
[ 1.687735] (align = 0x1000, id = 0, autobalance = 1, init = 0)
[ 1.698852] Managing the chunk [0xc9000000 - 0xd0000000]
[ 1.698852] (align = 0x1000, id = 1, autobalance = 1, init = 0)
[ 1.714181] Managing the chunk [0x3e801000 - 0x3eb00000]
[ 1.714181] (align = 0x8, id = 2, autobalance = 0, init = 1)
[ 1.724960] Initializing '3e801000.oalsramS'
[ 1.774133] Managing the chunk [0x3eb00000 - 0x3ec00000]
[ 1.774133] (align = 0x8, id = 3, autobalance = 0, init = 1)
[ 1.784914] Initializing '3eb00000.oalsramM'
[ 1.900160] CSI: driver ready -> CSI0 = enabled | CSI1 = enabled.
[ 1.983458] Load sbc board configuration
[ 1.987307] CGD: ready.
[ 2.095025] SError Interrupt on CPU2, code 0xbf000002 -- SError
[ 2.095028] CPU: 2 PID: 763 Comm: insmod Tainted: G O 4.19.31-rt18+g9efc51a #1
[ 2.095030] Hardware name: Freescale S32V234 (DT)
[ 2.095031] pstate: 20000005 (nzCv daif -PAN -UAO)
[ 2.095033] pc : SeqRamsInit+0x5c/0x130 [seq]
[ 2.095034] lr : SEQ_DRV_Setup+0x30/0xb0 [seq]
[ 2.095035] sp : ffffff800b4ebb30
[ 2.095037] x29: ffffff800b4ebb30 x28: 000000000000002f
[ 2.095041] x27: ffffffc07aedddd0 x26: ffffff8000c30550
[ 2.095044] x25: ffffff8000c30188 x24: ffffff80088e0000
[ 2.095047] x23: ffffff8000c30500 x22: ffffff8000c30000
[ 2.095051] x21: ffffff8000c30000 x20: ffffff8000c30000
[ 2.095054] x19: ffffff8000c30808 x18: ffffffffffffffff
[ 2.095057] x17: 0000000000000000 x16: 0000000000000000
[ 2.095061] x15: 0000000000000400 x14: 0000000000000400
[ 2.095064] x13: 0000000000000000 x12: 0000000000000001
[ 2.095067] x11: 0000000000026374 x10: 0000000001077b93
[ 2.095071] x9 : 0000000000000138 x8 : ffffffc07dfce040
[ 2.095074] x7 : 0000000000000000 x6 : ffffff8008895368
[ 2.095077] x5 : 0000000000000000 x4 : 0000000000000000
[ 2.095081] x3 : ffffff8008a45000 x2 : ffffff8000c30000
[ 2.095084] x1 : ffffff8008a66000 x0 : ffffff8008a65017
[ 2.095088] Kernel panic - not syncing: Asynchronous SError Interrupt

.

.

标记 (2)
0 项奖励
回复
1 解答
10,797 次查看
stefans
NXP Employee
NXP Employee

Root cause might be related to missing cse.bin. If the device is security enabled (which is true for latest SBCs) seq.ko will fail loading.

Best regards,

   Stefan.

在原帖中查看解决方案

5 回复数
10,798 次查看
stefans
NXP Employee
NXP Employee

Root cause might be related to missing cse.bin. If the device is security enabled (which is true for latest SBCs) seq.ko will fail loading.

Best regards,

   Stefan.

10,797 次查看
nskang
Contributor II

Dear Stefan Schwarz

many thanks for your answer.

I'm in a trouble still playing demo with SBC-S32V234 board. 

i can't anything with it.

i hope that you assist me to solve my issue.

Issue 1.

As you know My SBC-S32V234 board can't boot with Yocto binary Image which is downloaded from NXP web.

<You already answered about this issue>

but i can't make cse.bin file because i only have a u-boot.s32(Yocto) Image not Yocto source code. 

so, if you know that how to change device security option from enable to disable. please let me know. i will try.

Issue 2.

Always SBC-S32V234 board hangs with "Buffer overrun" message when executing a sample application(elf)

System Infomation

* u-boot.s32 : v2018.07_bsp23.0

  kernel : v4.19.59_bsp23.0

  10 kernel modules (viulite, jpegdcd,cam,csi,apex,h264dcd,h264enc,fdma,oal_cma,seq) are built manually

 * S32DS_Vision_Linux_v2.0_b170913.bin

 * application : isp_sonyimx224_h264enc_linux.elf (S32DS Project from Sample)


root@s32v234sbc:~# ./my_isp_sonyimx224_h264enc_linux.elf

**************************************************************
** H264 encoder demo
** Description:
** o Sony imx224 camera (on MipiCsi_0) expected as image input.
** o ISP generates histogram for AEC, converts pixel format from
** RGB to YUV420 and trigers H264 encoding.
** o H264Encoded stream data are located in SRAM.
**
** Usage:
** o 1 parameter: number of frames to be captured and encoded.
** o no params => 200 frames will be captured and encoded.
**
**************************************************************
**
** 200 frames will be encoded.
**
**************************************************************

Press Ctrl+C to terminate the demo.
[ 77.598909] Probing I2c client @ 0x1a on I2C bus #0.
[ 77.603780] Generic camera I2c driver added successfully.
VMAX = 745, Lines = 729, OB = 2
Framebuffer mapped at 0x7fb4922000.
*** Other error message received.
*** Sequencer error text:
Buffer overrun @4508:256

 

Best regards,

 Namsu,

0 项奖励
回复
10,797 次查看
nskang
Contributor II

Thanks.

i got it your said's mean.

but, i'm not sure that what shall i do.

i already said that i used yocto binary image from web.

how can i solve this problem.?

0 项奖励
回复
10,797 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi stefans‌

FYI. 

Do you know what might be wrong here?

Thank you!

Daniel

0 项奖励
回复
10,601 次查看
dakshina_dasari
Contributor I

I am also facing the same problem.

The solution is not clear.

Can you please elaborate -- how can i build the cse.bin? and where do i place it?

Also can i disable it for building the seq.ko?

 

Regards,

Dakshina

 

0 项奖励
回复