How to Detect Faces with NXP Vision Toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Detect Faces with NXP Vision Toolbox

6,012件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Face Detection

The following livescript uses MATLAB functionalities to simulate the face detection application. Face detection algorithm is implemented using Local Binary Patterns and Cascading Classifiers.
Read the input image.
inImgPath = 'data/face_detection.png';
inImgUMat = nxpvt.imread(inImgPath);
if isempty(inImgUMat)
    fprintf('Failed to open input image: %s.', inImgPath);
    return;
end
nxpvt.imshow(inImgUMat);
pastedImage_1.png
Define a face detector object.
width = uint32(640);
height = uint32(480);
fdetector = nxpvt.FaceDetector(width, height);
Apply the face detection algorithm on the grayscale image.
[bbox, l] = fdetector.GetFaces(inImgUMat);
Add the result on the original image.
outImgUMat = nxpvt.cv.rectangle(inImgUMat, bbox, [255, 0 ,0], 5);
nxpvt.imshow(outImgUMat);
pastedImage_2.png
ラベル(1)
0 返答(返信)