SPT3.x Basic Example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPT3.x Basic Example

3,491 次查看
__invited__gor1
NXP Employee
NXP Employee

Hi,

Our customer is utilizing MBDT(Model based Design Toolbox) in Matlab for simulation of SPT3.x in S32R45. However, we've got an error message when we run the basic example for SPT3.x provided in MBDT as a default. For example, when we run "example_fft8_spt31" it can't be finished with error message like the attached image. Error using spt31_sim_mex Error code is -5, and error message is: No such feature exists.

***Error in example_fft8_spt31 (line 70)***
***switch_spt(31);***

If we refer to error message, it seems we can't call switch_spt() properly. I've checked this error only happens over 3.x Please check this error also happens at your side and provide a solution.

0 项奖励
回复
0 回复数