How to quickly download programs into S32R274?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to quickly download programs into S32R274?

2,829件の閲覧回数
pingfang
Contributor III

Hello,

How to quickly download programs into S32R274 ?

The z4, z7_0 and z7_1 core are used in my project. But, it's not convenient to download programs to S32R274 (three .elf document, time-consuming ).

If I have hundreds of S32R  to be download, how can I do this well ?

Thank you .

0 件の賞賛
返信
2 返答(返信)

2,536件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi pingfang‌,

The S32R274 has a Boot-Assist-Module (BAM) that supports internal flash programming via a serial link (LIN /CAN).

Hence, you may want to investigate if the RAppID bootloader tool might be an option for you to program the executable in the the SoC. 

All that i know, is that RAppID bootloader utility tool can be controlled from command line (this is what we do for Model-Based Design Toolbox) to program applications in flash. This way you can build some scripts to automate your process.

Anyhow, before starting on that path you need to confirm with NXP Technical support if the S32R274 processor is supported by that tool or that are the plans for that.

Hope the hint will help you!

Daniel

0 件の賞賛
返信

2,536件の閲覧回数
pingfang
Contributor III

Thank you for your reply.

There is no S32R274 in the RAppID.

Could you explain it in detail? Is there any documents for flash programming  via a serial link (LIN /CAN)?pastedImage_1.png

Thank you .

0 件の賞賛
返信