CAN TX in S32R274

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN TX in S32R274

2,655件の閲覧回数
ansonan
Contributor I

CAN TX in S32R274

I USE THE CAN at loopback mode ,BUT 

always wait here  

  while (CAN_1.MCR.B.FRZACK & CAN_1.MCR.B.NOTRDY) {} /* Wait to clear */
                 /* Good practice: wait for FRZACK on freeze mode entry/exit */

the tx can't tx signal 

and the rx can't receive the signal

0 件の賞賛
返信
2 返答(返信)

2,504件の閲覧回数
ansonan
Contributor I

the flexcan  always in the Freeze mode? 

i don't konw why 

0 件の賞賛
返信

2,504件の閲覧回数
iulianbulancea
NXP Employee
NXP Employee

Hello,

Here on the Model-Based Design for RADAR community we handle questions regarding our toolbox or other MATLAB related questions. I think your question is best suited for the  S32 Design Studio community, so my advice is to ask it there (as I can not move it myself).

 

As an alternative you could open a ticket for technical support here (go to 'Go to Ticket').

 

Hope this helps,

Iulian.

0 件の賞賛
返信