Workshop challenges – 10 points Workshop Challenges – 6 points •Challenge 0: Boot Linux on UDOO •Challenge 1: ‘Hello World’ App on UDOO •Challenge 2: Led Blinking •Challenge 3: ATMEL – i.MX6 Communication Post-workshop Challenge – 4 points •Challenge 4: Connect a sensor to UDOO Project Development – 60 points •Each milestone has its score •Each milestone’s score is gained when: •The code is summited in the GIT repo •The video is send via email •Each day of delay will determine a loss of 5% from the milestone’s score •Bonus: 20%*Project_Development_Score Final Presentation – 30 points Judging Criteria Originality Execution Usability Documentation
查看全文