Rules

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rules

Rules

Workshop challenges – 10 pointschart.png

Workshop Challenges – 6 points

•Challenge 0: Boot Linux on UDOO

•Challenge 1: ‘Hello World’ App on UDOO

•Challenge 2: Led Blinking

•Challenge 3: ATMEL – i.MX6 Communication

Post-workshop Challenge – 4 points

•Challenge 4: Connect a sensor to UDOO

Project Development – 60 points

•Each milestone has its score

•Each milestone’s score is gained when:

•The code is summited in the GIT repo

•The video is send via email

•Each day of delay will determine a loss of 5%

from the milestone’s score

•Bonus: 20%*Project_Development_Score

Final Presentation – 30 points

Judging Criteria

        • Originality
        • Execution
        • Usability
        •   Documentation
No ratings
Version history
Last update:
‎03-17-2016 03:16 AM
Updated by: