p2020 PCIe linux kernel module reads 0xffffffff on BARs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p2020 PCIe linux kernel module reads 0xffffffff on BARs

3,959 Views
andreipetrukhin
Contributor I

I write my  pci driver for custom board on p2020. When I compile it for x86, it works fine, but when I compile it for my custom board, it reads only 0xffffffff on all BARs. I noticed, PCI bridge doesn't have any interrupt pin (like A, B, C, D) routed to IRQ 24. Could be my trouble in this? MSI is enabled in linux kernel.

lpci for PCI bridge

# lspci -s a000:00:00.0 -vv
a000:00:00.0 PCI bridge: Freescale Semiconductor Inc P2020 (rev 21) (prog-if 00 [Normal decode])
        Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR+ FastB2B- DisINTx-
        Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
        Latency: 0
        Interrupt: pin ? routed to IRQ 24
        Region 0: Memory at <ignored> (32-bit, non-prefetchable) [size=1M]
        Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
        I/O behind bridge: 00000000-00000fff
        Memory behind bridge: c0000000-dfffffff
        Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
        BridgeCtl: Parity- SERR- NoISA- VGA- MAbort- >Reset- FastB2B-
                PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
        Capabilities: [44] Power Management version 2
                Flags: PMEClk- DSI- D1+ D2+ AuxCurrent=0mA PME(D0+,D1+,D2+,D3hot+,D3cold+)
                Status: D0 NoSoftRst- PME-Enable+ DSel=0 DScale=0 PME-
        Capabilities: [4c] Express (v1) Root Port (Slot-), MSI 00
                DevCap: MaxPayload 256 bytes, PhantFunc 0
                        ExtTag- RBE-
                DevCtl: Report errors: Correctable+ Non-Fatal+ Fatal+ Unsupported+
                        RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                        MaxPayload 128 bytes, MaxReadReq 512 bytes
                DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr- TransPend-
                LnkCap: Port #0, Speed 2.5GT/s, Width x4, ASPM L0s, Exit Latency L0s <2us, L1 unlimited
                        ClockPM- Surprise- LLActRep- BwNot- ASPMOptComp-
                LnkCtl: ASPM Disabled; RCB 128 bytes Disabled- CommClk-
                        ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk- DLActive- BWMgmt- ABWMgmt-
                RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna+ CRSVisible-
                RootCap: CRSVisible-
                RootSta: PME ReqID 0000, PMEStatus- PMEPending-
        Capabilities: [100 v1] Advanced Error Reporting
                UESta:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                UESvrt: DLP+ SDES- TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
                CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
                AERCap: First Error Pointer: 00, GenCap+ CGenEn- ChkCap+ ChkEn-
        Kernel driver in use: pcieport

0 Kudos
Reply
0 Replies