Linux Kernel Programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Kernel Programming

Linux Kernel Programming

Linux Kernel Developing

U-boot and Kernel Compilation

  1. Get right toolchain for your platform.

            a. Ubuntu: sudo apt-get install gcc-arm-linux-gnueabi/gcc-arm-linux-gnueabihf

or

           b.  Get from linaro.org : wget -c https://releases.linaro.org/14.04/components/toolchain/binaries/gcc-linaro-arm-linux-gnueabihf-4.8-2...

   2. Get U-boot code source

    1. git clone http://git.denx.de/u-boot-imx.git
    2. make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi- wandboard_quad_config
    3. make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi-

   3. Get Kernel source with Wandboard support

    1. Wandboard repo:
      1. git clone https://github.com/wandboard-org/linux.git
      2. Select the right branch:
      3. git checkout wandboard_imx_3.10.17_1.0.0_beta    

                              or     

                           git checkout wandboard_imx_3.0.35_4.1.0

             b. Kernel Configuration ( load the wandboard  config )

                     make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi- wandboard_defconfig

                                    or

                           make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi- menuconfig

             c. Kernel Compilation

make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi-

     4. Prepare the sdcard:

            I. Copy the u-boot on the sdcard

      1. Determine the sdcard device name : sudo df -h
      2. sudo umount /dev/sdd*
      3. sudo dd if=/<path>/u-boot.imx of=/dev/sdd bs=512 seek=2

          II. Partitionating the sdcard

    • sudo fdisk /dev/sdd
      • o
      • n
      • p
      • 1
      • 2048
      • +1G
      • t
      • c
      • n
      • p
      • 2
      • 12288
      • +5G
      •   P
    • sudo mkfs.vfat -n KERNEL /dev/sdd1
    • sudo mkfs.ext3 -L RFS /dev/sdd2
    • cd /media/
    • sudo mkdir KERNEL
    • sudo mkdir RFS
    • sudo mount /dev/sdd1 KERNEL/
    • v. sudo mount /dev/sdd2 RFS/

         |||. Download a RFS and put on the sdcard

IV. Setup the u-boot:

    • run loadimage
    • run loadfdt
    • setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw
    • bootz ${loadaddr} - ${fdt_addr}

Kernel devices

Realise a kernel device controlled from user space. The following steps will be done on the virtual machine.

NEEDED: Get the Virtual Box softwarte:  https://www.virtualbox.org/wiki/Downloads

  1. Realize a kernel device which prints “Hello World” starting from you’re the attached code.

   a . First determine the kernel version from target platform:

    • uname –a
    • Get the kernel sources or kernel headers using one of the following methods. On the current virtual machine this step is already done.
      • For kernel headers: sudo apt-get install linux-headers-$(uname -r)
      • For kernel sources:
        • sudo apt-get install linux-source

   b. Now go to the directory tasks/kernel. Create a function void hello() which prints “Hello World”.  It should be called when the device is inserted.

   c.  Compile the module : make

   d.  Insert the module on the virtual machine : insmod lec_cdev.ko

   e.  See if the module  is inserted

    • lsmod
    • dmesg

   f. Remove the kernel module :  rmmod lec_cdev.ko

   2. Create the device lec_cdev using  mknod  /dev/lec_cdev c 243 0

   3. Implement the read function of the device in order to have the following effect:

  1. cat /dev/lec_cdev =>  print to infinit “a”
  2. Modify the previous module in order to be commanded using ioctl from userspace.
    1. In function lec_cdev_ioctl  detect the command sent  from userspace and

If command is

  • MY_IOCTL_HELLO prints “HELLO WORLD”;
  • MY_IOCTL_SET_BUFFER – prints the buffer received from userspace.
  • MY_IOCTL_GET_BUFFER – prints the data from the char device driver buffer
        HINT: use functions 
* copy_to_user(user_buffer, kernel_buffer, size)
* copy_from_user(kernel_buffer, user_buffer , size)
 
ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎09-10-2020 02:20 AM
更新者: