vmalloc: allocation failure: 4407240 bytes in LS1021ATWR Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vmalloc: allocation failure: 4407240 bytes in LS1021ATWR Board

7,662件の閲覧回数
vigneshr
Contributor III

Hi All,

I'm getting vmalloc() failure while trying to insert the module in the kernel. When I checked the vmalloc size, there is enough space for loading the module. Someone help me to resolve this issue,

Below is the log when inserting the module,

root@ls1021atwr:/lib# insmod wl.ko

vmap allocation for size 4411392 failed: use vmalloc=<size> to increase size.

vmalloc: allocation failure: 4407240 bytes

insmod: page allocation failure: order:0, mode:0xd0

CPU: 1 PID: 1213 Comm: insmod Tainted: P           O 3.12.37-rt51+ls1+gf488de6 #1

[<800107c9>] (unwind_backtrace+0x1/0x88) from [<8000e4e7>] (show_stack+0xb/0xc)

[<8000e4e7>] (show_stack+0xb/0xc) from [<8030492d>] (dump_stack+0x4d/0x60)

[<8030492d>] (dump_stack+0x4d/0x60) from [<8005c4fb>] (warn_alloc_failed+0x8f/0xb0)

[<8005c4fb>] (warn_alloc_failed+0x8f/0xb0) from [<80074bef>] (__vmalloc_node_range+0x113/0x134)

[<80074bef>] (__vmalloc_node_range+0x113/0x134) from [<8000eb4f>] (module_alloc+0x27/0x34)

[<8000eb4f>] (module_alloc+0x27/0x34) from [<8004af3b>] (module_alloc_update_bounds+0x9/0x42)

[<8004af3b>] (module_alloc_update_bounds+0x9/0x42) from [<8004b433>] (layout_and_allocate+0x4bb/0x56c)

[<8004b433>] (layout_and_allocate+0x4bb/0x56c) from [<8004b54b>] (load_module+0x67/0x9cc)

[<8004b54b>] (load_module+0x67/0x9cc) from [<8004bf63>] (SyS_finit_module+0x35/0x3e)

[<8004bf63>] (SyS_finit_module+0x35/0x3e) from [<8000c141>] (ret_fast_syscall+0x1/0x44)

Mem-info:

DMA per-cpu:

CPU    0: hi:  186, btch:  31 usd: 122

CPU    1: hi:  186, btch:  31 usd:  35

active_anon:981 inactive_anon:40 isolated_anon:0

active_file:2835 inactive_file:1727 isolated_file:0

unevictable:0 dirty:0 writeback:0 unstable:0

free:226520 slab_reclaimable:872 slab_unreclaimable:1300

mapped:583 shmem:69 pagetables:42 bounce:0

free_cma:0

DMA free:906080kB min:4064kB low:5080kB high:6096kB active_anon:3924kB inactive_anon:160kB active_file:11340kB inactive_file:6908kB unevictableo

lowmem_reserve[]: 0 0 0 0

DMA: 42*4kB (M) 8*8kB (UM) 9*16kB (UEM) 5*32kB (UEM) 3*64kB (UEM) 1*128kB (E) 6*256kB (UEM) 1*512kB (U) 2*1024kB (UM) 2*2048kB (UM) 219*4096kB B

4634 total pagecache pages

0 pages in swap cache

Swap cache stats: add 0, delete 0, find 0/0

Free swap  = 0kB

Total swap = 0kB

393216 pages of RAM

353699 free pages

7167 reserved pages

1514 slab pages

266830 pages shared

0 pages swap cached

insmod: ERROR: could not insert module wl.ko: Cannot allocate memory

size of Vmalloc () is ,

cat /proc/meminfo | grep -i vmalloc                                                                         

VmallocTotal:    1024000 kB

VmallocUsed:      142156 kB

VmallocChunk:     879548 kB

Even-though enough space is there, what could be the reason for this issue and how can I resolve  it..

Help is appreciated. Thanks in advance.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

6,500件の閲覧回数
johnbalian
Contributor I

Hello Vignesh, did you ever find the answer to this question?  I am having the same issue with the wl driver

John

0 件の賞賛
返信

6,500件の閲覧回数
vigneshr
Contributor III

Could someone help me ??

0 件の賞賛
返信

6,500件の閲覧回数
sinanakman
Senior Contributor III

Hi Vignesh, are you perhaps mistakenly trying

to allocate a huge chunk of memory during

module init ?

Regards

Sinan Akman

0 件の賞賛
返信

6,500件の閲覧回数
vigneshr
Contributor III

No Sinan.

0 件の賞賛
返信