unimplemented: '-mgeneral-regs-only' and floating point code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

unimplemented: '-mgeneral-regs-only' and floating point code

6,418 次查看
vigneshr
Contributor III

Hi All,

I'm cross compiling some third party SDK to ARM platform. While cross compiling I'm getting the below error.

"" sorry, unimplemented: '-mgeneral-regs-only' and floating point code ""

I was cross compiling for 64bit ARM platform. I'm using 64 bit tool chain aarch64-fsl-linux-*  and kernel also 64 bit.

Have anyone faced this issue before. If so suggest some ideas.

Thanks,
Vigneshwaran

标签 (1)
0 项奖励
回复
2 回复数

4,979 次查看
Pavel
NXP Employee
NXP Employee

NXP offers SDK 1.0 for the LS2080A processor:

https://www.nxp.com/webapp/Download?colCode=LS2080A-SDK-1-0&appType=license&location=null&Parent_nod...

.

Use this SDK for 64-bit ARM.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,979 次查看
vigneshr
Contributor III

Any Idea ?

0 项奖励
回复