unimplemented: '-mgeneral-regs-only' and floating point code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unimplemented: '-mgeneral-regs-only' and floating point code

6,360件の閲覧回数
vigneshr
Contributor III

Hi All,

I'm cross compiling some third party SDK to ARM platform. While cross compiling I'm getting the below error.

"" sorry, unimplemented: '-mgeneral-regs-only' and floating point code ""

I was cross compiling for 64bit ARM platform. I'm using 64 bit tool chain aarch64-fsl-linux-*  and kernel also 64 bit.

Have anyone faced this issue before. If so suggest some ideas.

Thanks,
Vigneshwaran

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

4,921件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers SDK 1.0 for the LS2080A processor:

https://www.nxp.com/webapp/Download?colCode=LS2080A-SDK-1-0&appType=license&location=null&Parent_nod...

.

Use this SDK for 64-bit ARM.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,921件の閲覧回数
vigneshr
Contributor III

Any Idea ?

0 件の賞賛
返信