need help: ls1043 DDR tuning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

need help: ls1043 DDR tuning

9,107 Views
Hmc510
Contributor II

soc:ls1043a

DDR:MT40A2G8VA-062E:B ,  x5, 4for 8GB,1 for ECC.

I use CW get a config files:

Hmc510_0-1680146733717.png

 

I tried two files to generate img

Hmc510_1-1680146792976.png

They all have problems running at BL2:

to use (0-2GB) DDR Data appears incorrect: (write ≠ read)

Hmc510_2-1680146840517.png

 

How should I solve it? Thanks

 

 

0 Kudos
Reply
9 Replies

9,027 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @Hmc510 

 

Can you please perform below validation with QCVS DDR tool.

 

1. Centering The Clock

2. Read ODT and Driver

3. Write ODT and Driver

 

Thanks

Khushbu

0 Kudos
Reply

8,974 Views
Hmc510
Contributor II

Hi

I unexpectedly solved this problem.CPU has been adjusted from 1.6G to 1.2G,the uboot startup.

I don't know why. SYSCLK & DDRCLK is 100M.

 

Hmc510_1-1680777117373.png

 

 

0 Kudos
Reply

9,025 Views
Hmc510
Contributor II

Yes, they all seem to have turned out very successful.

And I removed ECC(U20 & R146) chip from the board.Close ECC and regenerate configuration parameters; Still down in BL2.

And I tried the following CW configuration:

4GB: 1G8、8GB: 2G8.They all tested CW normally,hang up at BL2.

 

Hmc510_0-1680590904556.png

Hmc510_1-1680590967253.png

Hmc510_2-1680590975517.png

 

0 Kudos
Reply

9,014 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @Hmc510 

 

Can you please share boot logs in txt format.

 

Thanks

Khushbu

0 Kudos
Reply

9,010 Views
Hmc510
Contributor II

This is the startup log with ECC.

I tried to turn off OPTEE,It will also stop at BL2.

0 Kudos
Reply

9,066 Views
Hmc510
Contributor II

about MT40A2G8VA-062E:B I found a total of two documents online:

16gb_ddr4_x4x8_2cs_twindie.pdf  MICT_S_A0010972464_1-2574446.pdf

0 Kudos
Reply

9,071 Views
Hmc510
Contributor II

DDR PCB:

P05-DDR4.pdf

DDR 2G8 datasheet  MT40A2G8VA-062E:B:

MICT_S_A0010972464_1-2574446.pdf

 

Information supplement:

I modified the ATF code to test the DDR:

write data to 1K memory and then read back for verification. two messages were found:

  1. Some bits have changed
  2. CW read back data appears to be correct and ATF crc notify NG...(I'm sure there's no dizziness)
 

Hmc510_1-1680252520185.png

Hmc510_0-1680253294093.png

 

 

 

0 Kudos
Reply

9,098 Views
Hmc510
Contributor II

and CW test 0~2G is good :

Hmc510_0-1680148153652.png

 

 

0 Kudos
Reply

9,015 Views
Hmc510
Contributor II

@khushbur  This is where I obtain.CW test 0-2GB passed,The 0-2G test in BL2 is incorrect.

I also read back the DDRC register,They all have no problem.

0 Kudos
Reply