mmc0: Tuning failed on LS1046ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mmc0: Tuning failed on LS1046ARDB

1,664件の閲覧回数
prafulls
Contributor II

Hi Team,

    We were facing the mmc mount issue while bootup in LS1046ARDB. This issue come in between multiple reboot.  Please fine below console logs for the same & please do suggest the appropriate action/solution required for this.

 

0482 [ 3.556800] Freescale USDPAA process driver
90483 [ 3.560977] fsl-usdpaa: no region found
90484 [ 3.564823] Freescale USDPAA process IRQ driver
90485 [ 3.581027] optee: probing for conduit method from DT.
90486 [ 3.587919] optee: api uid mismatch
90487 [ 3.592338] mmc0: Tuning failed, falling back to fixed sampling clock
90488 [ 3.595073] u32 classifier
90489 [ 3.595074] Actions configured
90490 [ 3.595964] Initializing XFRM netlink socket
90491 [ 3.596268] NET: Registered protocol family 10
90492 [ 3.596820] Segment Routing with IPv6
90493 [ 3.596874] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
90494 [ 3.597169] NET: Registered protocol family 17
90495 [ 3.597181] NET: Registered protocol family 15
90496 [ 3.597209] Bridge firewalling registered
90497 [ 3.597275] 8021q: 802.1Q VLAN Support v1.8
90498 [ 3.597358] 9pnet: Installing 9P2000 support
90499 [ 3.597385] tsn generic netlink module v1 init...
90500 [ 3.597418] Key type dns_resolver registered
90501 [ 3.597893] registered taskstats version 1
90502 [ 3.598696] Btrfs loaded, crc32c=crc32c-generic
90503 [ 3.600499] iommu: Adding device 2c00000.edma to group 7
90504 [ 3.607323] i2c i2c-1: using dma0chan16 (tx) and dma0chan17 (rx) for DMA transfers
90505 [ 3.607326] i2c i2c-1: IMX I2C adapter registered
90506 [ 3.607410] iommu: Adding device 0000:00:00.0 to group 8
90507 [ 3.607638] pcieport 0000:00:00.0: Signaling PME with IRQ 67
90508 [ 3.607721] iommu: Adding device 0000:01:00.0 to group 8
90509 [ 3.607976] mhi 0000:01:00.0: BAR 0: assigned [mem 0x5040000000-0x5040000fff 64bit]
90510 [ 3.608279] [I][mhi_async_power_up] Requested to power on
90511 [ 3.609173] [I][mhi_async_power_up] Power on setup success
90512 [ 3.609186] [I][mhi_pci_probe] Return successful
90513 [ 3.609217] [I][mhi_fw_load_worker] Waiting for device to enter PBL from EE:INVALID_EE
90514 [ 3.609227] [I][mhi_pm_st_worker] Transition to state:PBL
90515 [ 3.609236] [I][mhi_fw_load_worker] Device current EE:PBL
90516 [ 3.609275] mhi 0000:01:00.0: Direct firmware load for fsm100xx/sbl1.mbn failed with error -2
90517 [ 3.609279] [E][mhi_fw_load_worker] Error loading firmware, ret:-2
90518 [ 3.609285] [I][mhi_runtime_idle] Entered returning -EBUSY
90519 [ 3.609742] input: gpio-keys as /devices/platform/gpio-keys/input/input0
90520 [ 3.609907] hctosys: unable to open rtc device (rtc0)
90521 [ 3.769468] mmc0: Hold on to use fixed sampling clock. Try SW tuning!
90522 [ 3.776330] VFS: Cannot open root device "mmcblk0p6" or unknown-block(0,0): error -6
90523 [ 3.784066] Please append a correct "root=" boot option; here are the available partitions:
90524 [ 3.792414] 0100 524288 ram0
90525 [ 3.792415] (driver?)
90526 [ 3.798505] 0101 524288 ram1
90527 [ 3.798506] (driver?)
90528 [ 3.804597] 0102 524288 ram2
90529 [ 3.804597] (driver?)
90530 [ 3.810688] 0103 524288 ram3
90531 [ 3.810689] (driver?)
90532 [ 3.816779] 0104 524288 ram4
90533 [ 3.816779] (driver?)
90534 [ 3.822869] 0105 524288 ram5
90535 [ 3.822869] (driver?)
90536 [ 3.826935] mmc0: Tuning timeout, falling back to fixed sampling clock
90537 [ 3.827155] mmc0: tuning execution failed: -110
90538 [ 3.827162] mmc0: error -110 whilst initialising MMC card
90539 [ 3.845386] 0106 524288 ram6

0539 [ 3.845386] 0106 524288 ram6
90540 [ 3.845386] (driver?)
90541 [ 3.851476] 0107 524288 ram7
90542 [ 3.851477] (driver?)
90543 [ 3.857568] 0108 524288 ram8
90544 [ 3.857569] (driver?)
90545 [ 3.863660] 0109 524288 ram9
90546 [ 3.863661] (driver?)
90547 [ 3.869751] 010a 524288 ram10
90548 [ 3.869752] (driver?)
90549 [ 3.875928] 010b 524288 ram11
90550 [ 3.875929] (driver?)
90551 [ 3.882106] 010c 524288 ram12
90552 [ 3.882106] (driver?)
90553 [ 3.888283] 010d 524288 ram13
90554 [ 3.888284] (driver?)
90555 [ 3.894461] 010e 524288 ram14
90556 [ 3.894461] (driver?)
90557 [ 3.900639] 010f 524288 ram15
90558 [ 3.900639] (driver?)
90559 [ 3.906821] 1f00 65536 mtdblock0
90560 [ 3.906821] (driver?)
90561 [ 3.913345] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
90562 [ 3.913348] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.19.90-rt35+g134788b16485 #1
90563 [ 3.913349] Hardware name: LS1046A RDB Board (DT)

 

Thanks,

Prafull

タグ(1)
0 件の賞賛
返信
0 返答(返信)