lsdk system reboot while kill -9 vpp&dpdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lsdk system reboot while kill -9 vpp&dpdk

1,666 Views
nxppenpals
Contributor II

We have a custom board with LS2160 CPU on it.
Operating System: NXP LSDK 2004 main
Kernel: 4.19.90
.vpp version :vpp v22.06.1-release
dpdk version :DPDK 21.11.2
DPDK EAL init args: --huge-unlink --huge-dir /run/vpp/hugepages --no-pci --in-memory --no-telemetry --file-prefix vpp
restool -v
restool v2.4 (10.30.0 compatible)
restool -m
MC firmware version: 10.36.0
We run vpp include dpdk plugin on it
As a beginner ,we are dealing with a critical problem.
When we use kill -9 to force VPP to quit,
the system will reboot immediately without any crash logs.
Is there any way to solve the problem?
Thanks for advice from experienced experts.
Regards,

0 Kudos
Reply
2 Replies

1,644 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,634 Views
nxppenpals
Contributor II

Thank you for your reply.
The ipsec feature is disabled in our vpp.
It seems that this bug can not cause system to  reboot.

0 Kudos
Reply