lsdk system reboot while kill -9 vpp&dpdk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lsdk system reboot while kill -9 vpp&dpdk

1,662 次查看
nxppenpals
Contributor II

We have a custom board with LS2160 CPU on it.
Operating System: NXP LSDK 2004 main
Kernel: 4.19.90
.vpp version :vpp v22.06.1-release
dpdk version :DPDK 21.11.2
DPDK EAL init args: --huge-unlink --huge-dir /run/vpp/hugepages --no-pci --in-memory --no-telemetry --file-prefix vpp
restool -v
restool v2.4 (10.30.0 compatible)
restool -m
MC firmware version: 10.36.0
We run vpp include dpdk plugin on it
As a beginner ,we are dealing with a critical problem.
When we use kill -9 to force VPP to quit,
the system will reboot immediately without any crash logs.
Is there any way to solve the problem?
Thanks for advice from experienced experts.
Regards,

标记 (5)
0 项奖励
回复
2 回复数

1,640 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,630 次查看
nxppenpals
Contributor II

Thank you for your reply.
The ipsec feature is disabled in our vpp.
It seems that this bug can not cause system to  reboot.

0 项奖励
回复