ls1046ardb uboot error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1046ardb uboot error

1,877 Views
hongyuanz
Contributor IV

 

It just prints out

U-Boot SPL 2021.04 (Nov 15 2021 - 18:13:58 +0800)
Initializing DDR....using SPD
DDR: failed to read SPD from address 81
Error: No valid SPD detected.  

 

0 Kudos
Reply
3 Replies

1,867 Views
hongyuanz
Contributor IV
0 Kudos
Reply

1,856 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could download LSDK 21.08 pre-built firmware image with the following command.

wget https://www.nxp.com/lgfiles/sdk/lsdk2108/firmware_ls1046ardb_qspiboot.img

Then deploy it on the alternate bank of QSPI flash on the target board.

=>tftp 0xa0000000 firmware_ls1046ardb_qspiboot.img

=>sf probe 0:1

=> sf erase 0 +$filesize

=>sf write 0xa0000000 0 $filesize 

 

0 Kudos
Reply

1,870 Views
yipingwang
NXP TechSupport
NXP TechSupport

Which version LSDK are you using? How did you generate the boot firmware image?

DDR initialization should be in ATF booting up stage not in u-boot.

0 Kudos
Reply