ls1046ardb uboot error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1046ardb uboot error

1,851 次查看
hongyuanz
Contributor IV

 

It just prints out

U-Boot SPL 2021.04 (Nov 15 2021 - 18:13:58 +0800)
Initializing DDR....using SPD
DDR: failed to read SPD from address 81
Error: No valid SPD detected.  

 

0 项奖励
回复
3 回复数

1,841 次查看
hongyuanz
Contributor IV
0 项奖励
回复

1,830 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You could download LSDK 21.08 pre-built firmware image with the following command.

wget https://www.nxp.com/lgfiles/sdk/lsdk2108/firmware_ls1046ardb_qspiboot.img

Then deploy it on the alternate bank of QSPI flash on the target board.

=>tftp 0xa0000000 firmware_ls1046ardb_qspiboot.img

=>sf probe 0:1

=> sf erase 0 +$filesize

=>sf write 0xa0000000 0 $filesize 

 

0 项奖励
回复

1,844 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Which version LSDK are you using? How did you generate the boot firmware image?

DDR initialization should be in ATF booting up stage not in u-boot.

0 项奖励
回复