ls1043a rdb run dpdk example problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1043a rdb run dpdk example problem

1,055 次查看
WXI
Contributor I
Hi all, 



I try to run lsdk 19.11 dpdk  myself custom-app example on ls1043ardb.

current thread affinity is set to F
legacy_mem 0
EAL: Detected 4 lcore(s)
EAL: Detected 1 NUMA nodes
EAL: Static memory layout is selected, amount of reserved memory can be adjusted with -m or --socket-mem
EAL: Multi-process socket /var/run/dpdk/rte/mp_socket
EAL: Selected IOVA mode 'PA'
EAL: Probing VFIO support...
EAL: VFIO support initialized
EAL: DPAA Bus Detected
dpaax: Unable to add mem-event handler
PMD: net: dpaa: fm1-mac1: 58:48:49:2f:fd:bd
PMD: net: dpaa: fm1-mac2: 58:48:49:2f:fd:be
PMD: net: dpaa: fm1-mac4: 58:48:49:2f:fd:bf
PMD: net: dpaa: fm1-mac5: 58:48:49:2f:fd:c0
PMD: net: dpaa: fm1-mac6: 58:48:49:2f:fd:c1


Does any one know how to fix it? Is dpaa can not boot with args “--legacy-mem”  ?



Regards
0 项奖励
回复
1 回复

1,033 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please set up Linux application debug environment, then debug into function dpaax_handle_memevents in drivers/common/dpaax/dpaax_iova_table.c in dpdk source code.

0 项奖励
回复