ls1028ardb ethernet (msi disabled) problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1028ardb ethernet (msi disabled) problem

1,347 次查看
pjw
Contributor II

We are developing custom board using ls1028.

The current problem is that Ethernet does not work when a PCI module that uses Marvell's chip is connected to the board


If  enter ifconfig after boot, eno0 and eno2 will not be checked.

After analyzing the log, it seems to be a problem to disable the msi side at the pci driver.

그림1.jpg

 


My question is, is there a way to operate ethernet regardless of msi?

Disabling msi seems to cause a problem with the irq_vector, and I wonder if we can set the irq_vector manually.

0 项奖励
回复
1 回复

1,319 次查看
andrei_skok
NXP Employee
NXP Employee

Our Software team has requested full kernel log and the information on LSDK release you are using.

0 项奖励
回复