[ls1028a] not bootable with UEFI flow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[ls1028a] not bootable with UEFI flow

1,982 Views
AristoChen
Contributor II

Hi

I was trying to boot ls1028ardb with UEFI flow, and there is an error in U-Boot: `Cannot use 64 bit addresses with SDMA`

 

 

U-Boot 2022.04-g18185931 (Sep 11 2024 - 13:15:30 +0800)

SoC:  LS1028AE Rev1.0 (0x870b0010)
Clock Configuration:
       CPU0(A72):1500 MHz  CPU1(A72):1500 MHz  
       Bus:      400  MHz  DDR:      1600 MT/s
Reset Configuration Word (RCW):
       00000000: 3c004010 00000030 00000000 00000000
       00000010: 00000000 018f0000 0030c000 00000000
       00000020: 020031a0 00002580 00000000 00003296
       00000030: 00000000 00000010 00000000 00000000
       00000040: 00000000 00000000 00000000 00000000
       00000050: 00000000 00000000 00000000 00000000
       00000060: 00000000 00000000 200e705a 00000000
       00000070: bb580000 00000000
Model: LS1028A RDB Board
Board: LS1028AE Rev1.0-RDB, Version: C, boot from SD
FPGA: v8 (RDB)
SERDES1 Reference : Clock1 = 100.00MHz Clock2 = 100.00MHz
DRAM:  3.9 GiB
DDR    3.9 GiB (DDR4, 32-bit, CL=11, ECC on)
Using SERDES1 Protocol: 47960 (0xbb58)
PCIe1: pcie@3400000 Root Complex: no link
PCIe2: pcie@3500000 Root Complex: x1 gen2
Core:  45 devices, 22 uclasses, devicetree: separate
WDT:   Started watchdog@c000000 with servicing (60s timeout)
WDT:   Started watchdog@c010000 with servicing (60s timeout)
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

EEPROM: Invalid ID (ff ff ff ff)
In:    serial
Out:   serial
Err:   serial
SEC0:  RNG instantiated
Net:   
Warning: enetc-0 (eth0) using random MAC address - d2:9b:a5:37:7b:b5
eth0: enetc-0
Warning: enetc-2 (eth1) using random MAC address - ca:57:11:de:de:cb
, eth1: enetc-2, eth2: swp0, eth3: swp1, eth4: swp2, eth5: swp3
Hit any key to stop autoboot:  0 
Trying load HDP firmware from SD..
switch to partitions #0, OK
mmc0 is current device
Device: FSL_SDHC
Manufacturer ID: 9f
OEM: 5449
Name: SD32G 
Bus Speed: 50000000
Mode: SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 28.9 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes

MMC read: dev # 0, block # 18944, count 512 ... 512 blocks read: OK
Loading hdp firmware from 0x00000000a0000000 offset 0x0000000000002000
Loading hdp firmware Complete
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
** Unable to read file / **
Failed to load '/'
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
Scanning disk [email protected]...
Scanning disk [email protected]...
Found 7 disks
ERROR: invalid device tree
Found EFI removable media binary efi/boot/bootaa64.efi
981992 bytes read in 44 ms (21.3 MiB/s)
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
WARNING could not find node vivante,gc: FDT_ERR_NOTFOUND.
Booting /efi\boot\bootaa64.efi
Cannot use 64 bit addresses with SDMA
Error reading cluster
** Unable to read file /efi/boot/grubaa64.efi **
Unexpected return from initial read: Device Error, buffersize 29D790
Failed to load image ぀¬ : Device Error
start_image() returned Device Error
## Application failed, r = 7
EFI LOAD FAILED: continuing...
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1...
** Unable to read file / **
Failed to load '/'
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
BootOrder not defined
EFI boot manager: Cannot load any image
Scanning mmc 1:2...
** Unable to read file / **
Failed to load '/'
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
BootOrder not defined
EFI boot manager: Cannot load any image
starting USB...
Bus usb@3100000: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
Bus usb@3110000: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb@3100000 for devices... 1 USB Device(s) found
scanning bus usb@3110000 for devices... 1 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found

Device 0: unknown device
Trying load from SD ...
switch to partitions #0, OK
mmc0 is current device
Device: FSL_SDHC
Manufacturer ID: 9f
OEM: 5449
Name: SD32G 
Bus Speed: 50000000
Mode: SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 28.9 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes

MMC read: dev # 0, block # 32768, count 81920 ... 81920 blocks read: OK
Wrong Image Format for bootm command
ERROR: can't get kernel image!
=> <INTERRUPT>
=> <INTERRUPT>
=> <INTERRUPT>

 

 

 

And I found that this commit added a new config called CONFIG_FSL_ESDHC_SUPPORT_ADMA2. After adding it in the ls1028ardb_tfa_defconfig, I am able to make ls1028ardb boot with UEFI flow without obvious issue, so I am wondering if NXP can confirmed that adding this config is the correct approach? and is there any concern or potential regression that it may brings?

 

thanks!

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,771 Views
LFGP
NXP TechSupport
NXP TechSupport

Dear AristoChen,

I have reviewed the commit you mentioned, it looks ok, but I can't guarantee that it could arising any concern.

On the other hand, please use the LLDP 6.1.55 and configure the DMAS fiel into the PROCTL register ( 15.4.12 Protocol control register, LS1028ARM Reference Manual)

0 Kudos
Reply

1,769 Views
AristoChen
Contributor II

Hi 

 

> please use the LLDP 6.1.55 and configure the DMAS fiel into the PROCTL register ( 15.4.12 Protocol control register, LS1028ARM Reference Manual)

 

Is this the document  that you want me to check? Could you please tell me which page to check? I can't find 15.4.12

Tags (1)
0 Kudos
Reply

1,751 Views
LFGP
NXP TechSupport
NXP TechSupport
find it on page 732 of the LS1028ARM reference manual
0 Kudos
Reply