lightdm error on ls1028

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lightdm error on ls1028

3,372件の閲覧回数
Eddy1
Contributor V

Hi:

I use lsdk to build the Ubuntu mate image, but there is no desktop. The following error occurs when I run it manually:

root@ubuntu:~# /usr/sbin/lightdm

** (lightdm:4852): WARNING **: 11:49:39.406: Seat type 'xlocal' is deprecated, use 'type=local' instead
Failed to use bus name org.freedesktop.DisplayManager, do you have appropriate permissions?

Could you give some suggestions?

0 件の賞賛
返信
3 返答(返信)

3,357件の閲覧回数
Pavel
NXP Employee
NXP Employee

Is this error message for flex-builder command?

 

Use the following command sequence for LSDK installing and building under Ubuntu 20:

sudo apt update

sudo apt -y upgrade

sudo apt-get install git

 

tar xvzf flexbuild_lsdk2108.tgz

source setup.env

 

flex-builder -i mkrfs -a arm64

 

flex-builder -c linux -a arm64

 

  1. flex-builder -i mkrfs -r ubuntu:mate -a arm64 //            # generate ubuntu userland, '-r ubuntu:main -a arm64' by default
  2. flex-builder -i mkbrfs -a arm64 -r ubuntu:mate 
  3. flex-builder -c apps -a arm64 ubuntu:mate -a arm64    # build all apps components
  4. flex-builder -i merge-component ubuntu:mate -a arm64  # merge app components into target userland
  5. flex-builder -i packrfs ubuntu:mate -a arm64          # pack and compress target userland as .tgz
  6. flex-builder -i mkfw -m ls1028ardb -b sd # generate composite firmware_ls1028ardb_uboot_sdboot.img
0 件の賞賛
返信

3,348件の閲覧回数
Eddy1
Contributor V

Hi:

Thank you for your reply. I use lsdk2012 to build Ubuntu mate on Ubuntu18.04. Do I need to be on the Ubuntu 20.04 host? In addition, I plan to install xfce4 desktop in Ubuntu main. I use apt get install xfce4 command to install it, and then run "X", but give the following complaints:

MESA-LOADER: failed to open mali-dp (search paths /usr/lib/aarch64-linux-gnu/dri:\$${ORIGIN}/dri:/usr/lib/dri)
failed to load driver: mali-dp
MESA-LOADER: failed to open kms_swrast (search paths /usr/lib/aarch64-linux-gnu/dri:\$${ORIGIN}/dri:/usr/lib/dri)
failed to load driver: kms_swrast
MESA-LOADER: failed to open swrast (search paths /usr/lib/aarch64-linux-gnu/dri:\$${ORIGIN}/dri:/usr/lib/dri)
failed to load swrast driver
couldn't get display device

Is lsdk2012 Ubuntu unable to install the xfce4 desktop? Could you give some suggestions?

タグ(1)
0 件の賞賛
返信

3,338件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use Ubuntu 18.04 for LSDK 2012. Use Ubuntu 20.04 for LSDK 2108.

It looks like that xfce4 is not available for Linux installed on the LS1028a board.

0 件の賞賛
返信