l2fwd dpdk application in LS1046ardb Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

l2fwd dpdk application in LS1046ardb Kit

1,433 Views
rashmikj
Contributor III

I am trying to configure all 4 cores to corresponding 4 ports of LS1046ardb kit for l2fwd application of dpdk.

l2fwd -c 0xf -n 1 -- -p 0xf

following error appears.

./l2fwd:process_portal_map(): Unknown error -1
dpaa: qman_thread_init failed on core 3 (lcore=3) with ret: -1
ioctl(DPAA_IOCTL_PORTAL_MAP): No such device
./l2fwd: process_portal_map(): Unknown error -1
dpaa: qman_thread_init failed on core 2 (lcore=2) with ret: -1

0 Kudos
Reply
1 Reply

1,424 Views
bpe
NXP Employee
NXP Employee


l2fwd tells you that it cannot find a free SW portal to assign to one or more cores.
Make sure you followed LSDK User Guide Section 9.2.4.1 paying attention to
the presence and the value of qportals and bportals kernel parameters and to the
correct Device Tree file selection.

Hope this helps
Platon

0 Kudos
Reply