l2fwd dpdk application in LS1046ardb Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

l2fwd dpdk application in LS1046ardb Kit

1,436件の閲覧回数
rashmikj
Contributor III

I am trying to configure all 4 cores to corresponding 4 ports of LS1046ardb kit for l2fwd application of dpdk.

l2fwd -c 0xf -n 1 -- -p 0xf

following error appears.

./l2fwd:process_portal_map(): Unknown error -1
dpaa: qman_thread_init failed on core 3 (lcore=3) with ret: -1
ioctl(DPAA_IOCTL_PORTAL_MAP): No such device
./l2fwd: process_portal_map(): Unknown error -1
dpaa: qman_thread_init failed on core 2 (lcore=2) with ret: -1

0 件の賞賛
返信
1 返信

1,427件の閲覧回数
bpe
NXP Employee
NXP Employee


l2fwd tells you that it cannot find a free SW portal to assign to one or more cores.
Make sure you followed LSDK User Guide Section 9.2.4.1 paying attention to
the presence and the value of qportals and bportals kernel parameters and to the
correct Device Tree file selection.

Hope this helps
Platon

0 件の賞賛
返信