how to change ddr4 config params on ls1043ardb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to change ddr4 config params on ls1043ardb

1,924件の閲覧回数
misakamikoto
Contributor III


Hi All:

     I'm working on changing ddr4 params on ls1043ardb,but I can't find the position where ddr4 params stand.Can somebody tell me where the dde4 params store?Txs!

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,697件の閲覧回数
hawkin
Contributor II

DDR4 params location in different place , timing params locate in : board\freescale\ls1043ardb\ddr.c    ddr_raw_timing[], udimm params locate in board\freescale\ls1043ardb\ddr.h  udimm0[]

0 件の賞賛
返信

1,697件の閲覧回数
Pavel
NXP Employee
NXP Employee

Usually u-boot provides DDR configuration on the board.

Change u-boot configuration using u-boot source code.

U-boot configuration file is located in the u-boot source folder: /include/configs. This folder contains the .h files for the different boards.

Find the ls1043a_commn.h file and CONFIG_SYS_FSL_DDR4 definition in this file.

This file is available in the attachment.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,697件の閲覧回数
misakamikoto
Contributor III

Txs,Pavel.But I mean I'm looking for the ddr4 config params header file,just like ddr timing or something else.I mean I want to change the ddr controller register value.So I think there must be a file just include this reg setting,doesn't it?

0 件の賞賛
返信